CORPORATE INFORMATION
Retrofit magazine recently recognized Greenheck model ECV-40 as one of the publication’s Top 25 Products of 2020. The eighth annual Top 25 Products, which appears in Retrofit’s January/February 2021 issue, celebrates the products that received...
The Greenheck Group announced today that it has signed a letter of intent to acquire Metal Industries, a leading manufacturer of grilles, registers, diffusers, and air terminal products used in commercial and institutional buildings. The addition...
Greenheck model DC-5, high volume low speed (HVLS) fan, received the gold level recognition as a Consulting-Specifying Engineer (CSE) 2020 Product of the Year. The award, voted on by the publication’s readers, was selected as the top product of the year in...
In a typical year, Greenheck hosts hundreds of people from around the world at its Schofield, Wisconsin campus for the company’s extensive HVAC University training programs. In 2020, COVID-19 quickly put a temporary halt to that. However, not even a pandemic could prevent Greenheck from...
Greenheck recently expanded its louver manufacturing capacity with a new 120,000-square-foot facility at its Shelby, North Carolina campus. The expansion significantly increases Greenheck's overall louver manufacturing footprint and supports the company's focus on...
Model DC-5 high volume low speed (HVLS) fan has won Engineered Systems’ 2020 Commercial Comfort Product of the Year Award in the IAQ/Ventilation category. Winners were officially announced in the...
Consulting Specifying Engineer (CSE) has named the Greenheck model DC-5 as a finalist for its Product of the Year award, in the HVAC category. The publication uses the award to highlight new products in the HVAC, fire/life safety...
FANS
Greenheck direct drive square inline fans now incorporate mixed flow wheel technology for a unique combination of high efficiency, low sound and ease of installation in a square housing design. AMCA certified for sound and air performance, mixed flow model SQ is...
Greenheck has added three-phase motors to its line of energy efficient Vari-Green® electronically commutated (EC) motors. The new three-phase motors accept 208-230V and 460V power supply and are available in sizes ranging from...
Greenheck’s new ceiling radiation damper model CRD-320WT, combined with select models of Greenheck ceiling exhaust bathroom fans, adds even more code-compliant options for wood truss applications. The CRD-320WT damper is UL approved for...
Greenheck’s line of high-volume low-speed (HVLS) fans continues to grow with the addition of model DC-5, a five-blade HVLS fan incorporating a sleek, lightweight design. DC-5 fans weigh less than 100 pounds and feature...
LABORATORY EXHAUST SYSTEMS
Greenheck’s Vektor®-H laboratory exhaust fans are now available with a reduced maintenance direct drive fan design for high efficiency operation, lower sound levels, and reduced long-term operating costs. The Vektor-H is a...
DAMPERS
Greenheck has introduced a round industrial control damper to accommodate higher velocities and pressure. Model HCDR-450 is rated for velocities up to 7000 fpm and pressure up to 30 in. wg, and withstands temperatures from...
Greenheck recently redesigned its AMD line of Air Measuring Dampers that combine an accurate airflow measuring station and a low leakage control damper into one compact unit. The differential pressure Air Measuring Station (AMS) now includes...
Greenheck has introduced two new heavy-duty industrial control dampers for high temperature applications. Models HCD-324 and HCD-524 feature a high temperature blade design to control...
Greenheck’s latest electric duct heater, model IDHE-O with a NEMA 4 enclosure, is UL listed for outdoor applications. The IDHE-O allows for multiple mounting positions where the control cabinet can be installed...
LOUVERS
Greenheck’s ESD-635HP, a 6-inch deep stationary drainable blade louver, is designed to provide high volume air flow and superior resistance to water penetration. The high-performance ESD-635HP incorporates drain gutters in the head member and...
DEDICATED OUTDOOR AIR SYSTEMS (DOAS)
Greenheck’s line of Dedicated Outdoor Air Systems (DOAS) for high percentage and 100% outside air continues to grow with the addition of two new models. Pre-engineered rooftop ventilator models RV-75 and RVE-150 with energy recovery offer...
MAKE-UP AIR
ENERGY RECOVERY VENTILATORS